7/16/2015 5:35 PM | |
Joined: 12/18/2014 Last visit: 5/4/2024 Posts: 32955 Rating: (4073) |
Yes, it is true that data log records each time the configured operand when the EN input 1 signal, but only for one cycle. You can, for example, at constant intervals make a pulse triggering, as well as through events, such as when an input signal 1 has. But you must make sure that the break between 2 events is at least 500 ms. If the time is small, the configured data is not recorded. AttachmentData_Log.zip (180 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on