6/25/2018 10:31 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
hi, yes, I-device communication should be possible. When one of the two communication-partner is not available it is shown on the other and you can react by programming the called OBs. There´s a application sample, but it shows mainly the S7-1500 controller in TIA: Configuration and Application of the PROFINET I-Device Function With Sinumerik you are working with Step7-Classic, so I guess the guidance in the following manual is more practicable for you: SIMATIC PROFINET System Description chapter 4.8 hope this helps, regards, |
FCK WAR! |
|
Follow us on