10/20/2009 2:44 PM | |
Posts: 6 Rating: (0) |
Please help me! We are the bakery from Serbia and we have a LOGO 24R relay 6ED10521HA000BA0 on the pastry cutting mashine. After the power lost somehow the program has been erased. The machine is from Pietroberto Italy and they send me this lsc file but i can not upload it because we don't have a newer version of LOGO and they don't have the old version of program. Can you please help us somehow or send us the correct program for this LOGO? I'm sending you the lsc file and below are errors when i try to upload the file i have from Italy. Can this program convert for the old version of LOGO? Thank you! *** 10/16/09 9:25 PM PASSO_PASSO.lsc *** Determine LOGO! Resources used: Function Blocks 7/130 REM 0/60 Digital Inputs 1/24 Digital Outputs 4/16 Flag 1/24 Analog Inputs 0/8 Text Box 0/10 Analog outputs 0/2 Program memory 76/2000 Block names 0/64 Analog flags 0/6 Cursor keys 0/4 Shift register 0/1 Shift register bits 0/8 Open connectors 0/16 Maximum nesting depth: I1-B002-B007-B004-Q3 The following LOGO! can be used: 0BA4.Standard 0BA5.Standard 0BA6.Standard 0BA6.ES3 *** 10/16/09 9:25 PM PASSO_PASSO.lsc *** Device selection The following devices cannot be used: 0BA0.Standard : M1 [Flag] May not be used 0BA0.L : M1 [Flag] May not be used 0BA0.LB11 : M1 [Flag] May not be used 0BA1.Standard : B005/3 Input inversion not supported 0BA1.L : B005/3 Input inversion not supported 0BA1.LB11 : B005/3 Input inversion not supported 0BA2.Standard : B005/3 Input inversion not supported 0BA2.Standard Analog: B005/3 Input inversion not supported 0BA2.L : B005/3 Input inversion not supported 0BA2.LB11 : B005/3 Input inversion not supported 0BA3.Standard : B005/3 Input inversion not supported AttachmentPASSO_PASSO.zip (547 Downloads) |
Last edited by: MOKA at: 10/20/2009 2:45 PM |
|
10/23/2009 3:23 PM | |
Posts: 6 Rating: (0) |
We have external timer on this machine, where we can set the number of sec.- interval beetween cuts. |
10/23/2009 4:43 PM | |
Posts: 661 Rating: (123) |
OK, this was a misunderstanding. So it seems the supplier sent a complete wrong program. Is it not possible to get a correct working version from him? For me, it´s not easy to understand how the machine is working in detail - what the LOGO! inputs and outputs have to do and when. Perhaps you know ? I mean: At input #1 pulses come in. With the first pulse it seem as if Q1 has to be switched on. Shall output #Q1 stay 1, until the next pulse will come (which shall enable output #2)? I tried this in the attached version. But in this version i do not know how to stop the sequence again. Is there another input #2 for"OFF"? Perhaps you can describe step by step, otherwise it´s hard. AttachmentPASSO_PASSO.zip (419 Downloads) |
10/24/2009 10:55 AM | |
Posts: 6 Rating: (0) |
With your last lsc file when i turn on the machine, the knife is NOT going up - Q2 is off! Here in attach you can find detail sheme for the cutting tool. I'm sorry but it is in Italian. And also i will send my program. When i start my program the logic is good, but the knife will not go all the way down in 4 of 10 cases or random.
AttachmentPiertoberto.zip (527 Downloads) |
10/24/2009 10:57 AM | |
Posts: 6 Rating: (0) |
Here is my experimental lsc file
Attachmentmoka.zip (462 Downloads) |
10/24/2009 7:51 PM | |
Joined: 12/27/2006 Last visit: 7/7/2024 Posts: 1197 Rating: (113) |
Here a have a program for you. Ill hope it works good When its not good, please make a better working-scription off the machine Attachmentmoka2.zip (457 Downloads) |
Last edited by: Toeternietoe at: 10/24/2009 7:58 PM |
|
Follow us on