1/13/2023 7:28 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi AutoGen_2706, you are right, normally if the faceplate jumps wouldn't work, it has something to do with the server package for example if you use the OS simulation. But if it's working in one language and another language not then it can't be the server package. I only have one idea. How long did you wait after the change of the language? If you change the runtime language of PCS 7 it can take up to 2-3 minutes after WinCC has changed the language completely. If you wait longer then 5 minutes, after you change the language I would create an Support Request, because the normally the faceplate jump has nothing to do with the language, the script for the faceplate jump will not change with the language setting. With regards |
This contribution was helpful to1 thankful Users |
Follow us on