11/21/2024 7:09 AM | |
Joined: 11/8/2024 Last visit: 12/16/2024 Posts: 4 Rating:
|
Hello Everybody, I have been testing the IOT2050 Basic Version (6ES7647 - 0BA00 - 0YA2) for about two weeks now. Last week I set it up with the example Image V1.3.1 (IOT2050_Example_Image_V1.3.1), which I downloaded from the official site. The setup via SD Card was quite easy and I followed the Instructions of this Post:How to setup the IOT2050 with Example Image - 238945 - Industry Support Siemens. After that I did the following steps:
Therefore I executed the following commands:
--> to this point I was still connected via SSH Client (I used PuTTy)
Therefore I executed the following commands:
--> After doing so the status showed Active when I executed "sudo systemctl status xrdp" and I could connect via Windows remote desktop from my engineering station.
(For Installing Grafana I followed their Instructions fromDownload Grafana | Grafana Labs)
This ia about all the configuration I did on the device. Now my problem is that after I did those last 3 changes the device would not boot anymore. When I tried to reboot the stat LED just stayed red. I decided to set the device up again from the beginning as I could not get it to boot. But since this happened, the IOT is behaving super weird. It often does not boot at all even with a whole new basis image (I tried two other new SD-Cards as well). When it recognizes the SD card and continues to boot then it is super slow (I am talking about 10 minutes for the boot process). Also new Errors occured: when I tried to install packages it often says something like
So installing anything on the device really got a pain, as it also seems like the download is way slower than before even though I am using the same connection. Also unpacking the packages when trying to install something just takes ages. The problem with the read-only file system can be solved by simply rebooting, where the problem comes into play that only about every tenth reboot actually suceeds, and the device boots. I would really appreciate any help with the device as I think I already tried out as much as I can but cannot get it to work propperly again. |
Last edited by: AutoGen_8327353 at: 11/21/2024 11:02:59 |
|
11/25/2024 12:57 PM | |
Joined: 11/8/2024 Last visit: 12/16/2024 Posts: 4 Rating:
|
Hello udae, thanks for your reply! I got the IOT up and running again (still very slow) and these are the Outputs/informations for you: Check your system logs the output of dmesg | grep -i "error" is the following:
the output of journalctl -b is very long so I will just attach a file with the output. Note that I only coppied the output from today because there were also some logs from July which I think might not be helpful. What is also strange is that it says Nov 19 at about 15:00 whereas these outputs should actually be from Nov 25 (today). Verify your Hardware and Image: I am using a 16GB micro SD Card with class 6. Sadly I cannot figure out the brand, but I have also tried a "Platinum micro SDHC Card high performance" Class 6 with 8GB from which the device does not boot at all. Fun fact: the 8GB card which is now not booting anymore was the card I set the device up with in the first place where everything was stilling running fine. I used Win32DiskImager to write the Image. I also tried to figure out the exact version of the Firmware but executing fw_printenv fw_version just results in
It says FS:07 on the device - So I am guessing from this post Overview about FS states of IOT2050 - 273280 - Industry Support Siemens that it might be firmware version V1.3.1. Read only file system: Sadly I have not been able to reproduce the read-only file system error as I do not really have the time to wait two hours for the IOT2050 to install something right now. After remounting the file system the output was as follows:
I appreciate all kind of help!
AttachmentLog.txt (143 Downloads) |
Last edited by: AutoGen_8327353 at: 11/25/2024 13:01:02Last edited by: AutoGen_8327353 at: 11/25/2024 13:04:32 |
|
11/25/2024 2:21 PM | |
Joined: 3/12/2024 Last visit: 8/15/2025 Posts: 183 Rating:
|
Hello, you can also connect the IOT2050 via DP cable to a monitor to see the full logs (the option to capture these logs into a file are a bit limited in this way). But maybe you can get some information about the not-booting system. We are using the FTDI USB to TTL UART cable if you're thinking about getting one for your IOT2050
|
Last edited by: udae at: 11/25/2024 14:22:13 |
|
Follow us on