11/29/2011 9:54 AM | |
Joined: 6/5/2009 Last visit: 10/4/2024 Posts: 151 Rating: (0) |
himark1507, Thanks for the reply. For now the issue does not seem to bother anyone as the plant is running smoothly and the customer is'nt interested in Step 7. FYI the FC that was mentioned did not have any siemens related blocks, nor did any part of the PCS 7 project have any blocks from PCS 7 library. Everything was customised. I can have a go at the method that you suggested byt using Save As, but in that case all the instant DB's related to the blocks are bound to change ...... So I assume that this would force us to re-do the whole project as all the structures in the OS are not formed through the Attribute "s7_m_c". So that really puts us back. Any ways thanks for the reply. regards, Grim Reaper.
|
Follow us on