7/2/2013 9:49 AM | |
Posts: 9 Rating: (0) |
hello...is it possible to link the function keys on the ktp400 basic panel with logo 7? if yes, a little tutorial would help thx
|
7/2/2013 10:39 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hello, Perhaps this link might help: http://support.automation.siemens.com/WW/view/en/56348902 Best regards, Wizard |
7/2/2013 10:41 AM | |
Joined: 11/23/2011 Last visit: 4/17/2024 Posts: 202 Rating: (32)
|
Hello tokaig, when you connect the function key with a flag in your programm, then you can configure this flag, f.e. M1, in the tag table of TIA Portal with the relavant adress (M0.0) and access thus the signal of the function key. Here is also an interesting example application about LOGO!-HMI connection with an example code for LOGO! and HMI-Panel: http://support.automation.siemens.com/WW/view/en/68585344 I haven't used direct linking of function keys to HMI before, so I can'tmake a statement about this. Greetings, KM_AS |
7/3/2013 10:13 AM | |
Posts: 9 Rating: (0) |
thank you a lot KM_AS ...i finally did it and everything is working fine |
This contribution was helpful to1 thankful Users |
1/19/2018 1:13 PM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7957 Rating: (162) |
New question published by TIA 13 is split to a separate thread with the subject Not able to create retentive variables. Best regards |
Last edited by: Jen_Moderator at: 1/19/2018 1:15:52 PMInserted right headline. My Forum is the place to personalize your profile, |
|
Follow us on