1/23/2014 9:17 AM | |
Joined: 4/24/2006 Last visit: 4/30/2024 Posts: 8628 Rating: (1147) |
Hello, If you purchase a starter package of KTP400 Comfort. It is possible to connect to LOGO 0BA7. And a Comfort panel can log data. I guess you have seen this link: how do you establish a connection between a LOGO! 0BA7 and an HMI Panel? Best regards, Wizard |
1/23/2014 9:39 AM | |
Joined: 4/24/2006 Last visit: 4/30/2024 Posts: 8628 Rating: (1147) |
Hello, It is possible to log data, this can be on a Memory card in HMI panel. Or you can log data on a directory of PC connected to the Ethernet. Perhaps this thread might help: /tf/WW/en/Posts/100797 Best regards, Wizard |
1/23/2014 9:53 AM | |
Posts: 8 Rating: (0) |
Wizard, great, thank you, just what I was looking for! Regards, 7Tech7 |
1/23/2014 10:22 AM | |
Joined: 4/24/2006 Last visit: 4/30/2024 Posts: 8628 Rating: (1147) |
Hello, That document described how to connect a Panel to the Ethenet network. You can not log data using a Basic Panel, you need a Comfort panel. See the following link: What are the functional differences between the different SIMATIC panels? Best regards, Wizard |
Follow us on