8/21/2018 10:31 AM | |
Posts: 45 Rating: (0) |
As a beginner in LOGO controllers I do have a challenge
The job is to copy an excisting program from LSC V8.1 for a new equipment and edit it for some changes in the I/O. The new LOGO bought is of course the newest version "6ED1 052-1FB08-0BA0" (230Vac) instead of the older version "6ED1 052-1HB00-0BA8" (24Vdc) and according info it should be programmed with LSC V8.2 I started with the excisting project in LSC V8.1, without replacing the LOGO. After editing and saving the project now I'm ready to convert it to LSC V8.2 and 'replace' the LOGO for the new bought one. But there it stops for me.
I've installed the LSC V8.2 at my VM with WinXP-sp3, it looks like it is working. But till now I didn't connect the LOGO to my (VM)-PC. Regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/21/2018 11:26:33 AMNew subject after splitting |
|
8/21/2018 11:15 AM | |
Posts: 45 Rating: (0) |
Thanks. But why should the new LOGO V8.2 be programmed in LSC V8.2? Regards, |
Follow us on