2/3/2025 5:37 PM | |
Joined: 1/31/2023 Last visit: 9/8/2025 Posts: 2 Rating:
|
Hello, Would you be able to confirm that the Mindconnect IoT2050 is compatible with the 10 x DI Arduino Shield (6ES7647-0KA02-0AA2) please? I can see the original post says it is incompatible but I have seen some conflicting info online. Thankyou! ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 02/04/2025 07:38:41New subject after splitting |
|
2/4/2025 1:08 PM | |
Joined: 3/12/2024 Last visit: 8/15/2025 Posts: 183 Rating:
|
Hello Arnoldsmith, theInput Module 6ES7647-0KA02-0AA2isofficially not compatible with the IOT2050. It's specifically designed for the SIMATIC IOT2020 and IOT2040. But the IOT2040 and IOT2050 using the same Arduino Uno R3 Pinout. Please refer to this pinout. I successfully tested the 10xDIs on a IOT2050 Advanced and Example Image:
Please keep in mind that it is officially incompatible - but it seems usable with the IOT2050. Besides that there is no cover for the IOT2050 with the 10x Input Module! My tests were done with Example Image and not on an IOT2050 - It's not possible to 100% transfer these results to the MindConnect IOT2050 - I also don't know how these inputs can be handled in the Asset Manager. As it is not officially tested an implementation would be on your own risk. |
This contribution was helpful to
1 thankful Users |
2/7/2025 10:20 AM | |
Joined: 3/12/2024 Last visit: 8/15/2025 Posts: 183 Rating:
|
Hey Arnoldsmith, I was in touch with the colleagues from the MindConnect devices. The only SIMATIC I/O Shield supported by the MindConnect IOT's (2040 & 2050) is the SIMATIC IoT2000 Input / Output Module 6ES7647-0KA01-0AA2. The SIMATIC IoT2000 Input Module Sink/Source 6ES7647-0KA02-0AA2 is not supported by the MindConnect IOT's (also not by the MindConnect IOT2040!). It's not possible to use it as it is not possible to configure it within the Asset Manager of the device. The Input Module Sink/Source is only supported with a default SIMATIC IOT2020 and IOT2040 (and also running on IOT2050 as mentioned above - but not supported). I'm sorry for the negative feedback. BR |
This contribution was helpful to
1 thankful Users |
Follow us on