4/13/2015 6:24 PM | |
Posts: 94 Rating: (0) |
any expert can help me about that ? |
4/14/2015 7:23 AM | |
Joined: 2/6/2009 Last visit: 5/7/2024 Posts: 938 Rating: (118) |
Hi Mohamed, What do you mean by LINK? Are you referring to Modbus Query to Next Slave with different parameters? If So, Here is the link for "Modbus Sample Project' by which we can achive queries to multiple slaves with different parameters. Complete description about how to used the Sample project is in the linked thread. Revert back for any further queries. |
_______________________________________________________________ |
|
4/14/2015 1:21 PM | |
Posts: 94 Rating: (0) |
YES link mean make program referring to Modbus Query to Next Slave with different parameters |
4/14/2015 2:08 PM | |
Joined: 2/6/2009 Last visit: 5/7/2024 Posts: 938 Rating: (118) |
Hi,
You can download the Modbus Sample Project from the given link and use it. The sample project is done for Modbus RTU (RS485) which suites your requirement. |
_______________________________________________________________ |
|
This contribution was helpful to1 thankful Users |
Follow us on