8/23/2017 8:28 PM | |
Joined: 7/28/2015 Last visit: 3/21/2024 Posts: 72 Rating: (1) |
Hi all I have one issue how to calculate the oil liter from the tank to the Oil Genset motor engine. The Diesel motor generator use around 105 Liter oil X hour. The diesel generator have embedded one circulation oil pump that continue loading from the tank and return back the unused oil to the tank. This mean one pipe for loading oil and t one pipe to return oil on tank, the difference oil is used from the engine. I will use the Oil flow sensor with turbine, where 100 click = 1 Liter. I try to make one schematic with 2 click flow sensor and the counter and the Input and Output counter are working. The problem is that I can not calculate the difference liters used from the engine With the analog matematic operation seem working, but is not the correct way. it is available a digital matematic operation? Example: Loading 50 Liters, return 20 liters= 30 liters used from engine. How to resolve this? Then I need to know how much liters: X hour, X day, X month. Thanks for the help AttachmentOil Liter Counter.zip (193 Downloads) |
8/24/2017 12:28 PM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
I have make a programm for you that stores the oil in 2 days You must change B004 Value 3 must by 100 (Divide by 100 because 100 pulsen = 1 liter) And take a Clock that give an output at the time you wish to reset the daytimer on the time you wish instead of input I3. This is only for testing Oh, and I1 must count more than I2 (In/Out) otherwise you get negative values of your oil AttachmentOil2.zip (197 Downloads) |
This contribution was helpful to1 thankful Users |
8/25/2017 10:58 PM | |
Joined: 7/28/2015 Last visit: 3/21/2024 Posts: 72 Rating: (1) |
Hi, I try to make this update... give a check. On this way is possible adding how many schedule timers as we like. My timers are set as 1 and 2 minute, just for fast example, then need to change with the correct time. Set the i3/i4 with frequency 150/90Hz mode just for fast running. let me know AttachmentOil Liter CounterV2.zip (249 Downloads) |
Follow us on