8/18/2012 10:46 AM | |
Posts: 21 Rating: (0) |
Dear Experts, ES/OS Configuration in ourProject: I’m creating a project using PCS7 Wizard in Simatic Manager.(One AS station and one ES Station). And develop all my logic and graphics. OS Configuration: 1. Importthe ES station and change the name to OS1. 2. InOS1 – Hardware Configuration I give the corresponding CP1613 MAC address ofOS1. 3. Compilethe project using Netpro and download the project to AS. 4. Copythe total project from Engineering station and put into Operating Station 1. 5. InOS1, open the station configuration and import the corresponding OS1 XDBs. 6. Openthe WinCC explorer and activate the project. The above procedures are correct or not for creating OS. I’ve a problem during that time. The License was expired message will come. At that time the POs goto demo mode in operating system. After deactivate the project it comes to 1000 POs. The same procedure I was following up all the Operating station. The same license problem was arrived all the operating station. Here no ip address communication, all are MAC addresscommunication. All systems are stand alone. Now Engineering station only communicate to AS. Kindly find the attached our system configuration diagramand screen shots of error. Kindly provide the solution for this issue. AttachmentOS Configuration Error.zip (71 Downloads) |
8/23/2012 5:56 AM | |
Posts: 21 Rating: (0) |
Dear JOTST, If i try to change Multiuser project to single user project. But it is not change. So only i ask my configuration procedure is correct or not. |
8/23/2012 7:23 PM | |
Joined: 11/15/2009 Last visit: 2/5/2024 Posts: 380 Rating: (47) |
Dear venkatvetri, Your configuration procedure is not typical for PCS 7. FAQ http://support.automation.siemens.com/WW/view/en/24023824 can help you. Regards |
Follow us on