8/1/2018 11:50 AM | |
Posts: 1368 Rating: (126) |
Hello, do you also tried the ID for the "IO-Device" means : 432 |
8/1/2018 12:19 PM | |
Posts: 1368 Rating: (126) |
Hello, please have a look to my post there is a data record application in SIOS available, also using RDREC. This application you can try to read out some data out of your PN device just for testing. |
8/1/2018 2:51 PM | |
Posts: 1368 Rating: (126) |
Are you sure, your Device is PROFINET and correctly integrated in TIA? |
8/1/2018 3:05 PM | |
Joined: 4/28/2015 Last visit: 4/5/2024 Posts: 66 Rating: (4) |
I installed GSDML file and the drag and dropped from HW catalog into TIA network view. Also as you can see from my first img diagnostics of the device is OK. Is it possoble that i made error in the begining of my developing. I have one device with Profinet interface and with gsdml file. But ussualy with another devices after installing i had inputs/outputs adresses and was abble to recieve data. But now i have a new type for me: without any IO adresses and with several HW Ids. Datsheet for the chip on this device Link I am realy need your help! |
Follow us on