3/7/2007 12:48 PM | |
Posts: 5 Rating: (1) |
Dear members, presently running on S5 115U with CP5431 card (6GK15431AA01) (S5 program attached) communicating with Profibus FMS with third party weighing controller (Make : Pfister Can System Controller). We had tried to communicate S7 and third party device (Make : Pfister Can System Controller) with above mention hardware, it reads active nodes attached to Profibus FMS but shows following error during data read operation. FMS connection 1 : Negative acknowledgment from layer 2 (status 17: ) during connection establishment to node with profibus address node 2 (Snapshot attached). Kindly help us in the following questions : Q1: what are the steps for configuring S7 to communicate with third party device on profibus FMS? Q2: what type of information is needed from third party device (Pfister) ? Q3: Sample program of S7 profibus FMS communication with CP 343-5 ?
AttachmentS5 Program.zip (772 Downloads) |
Follow us on