9/5/2024 9:02 PM | |
Joined: 8/23/2024 Last visit: 2/22/2025 Posts: 3 Rating:
|
Hi everyone! Before I spend many hours on trying program my PLC I need to ask you guys if is possible to create the program for the application where is two sensors (On the moving conveyor) and one switch. When the product is seen by first sensor , the timer starts and the second sensor it stops it. The switch is to reset that time( length of the product). Can I use that block with the counted time somewhere else. For example make a comparison whe if the time wasn’t met the product will be rejected. Application could be used for checking the length of the product where the speed of the conveyor is constant. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/06/2024 09:03:48New subject after splitting |
|
9/6/2024 3:53 AM | |
Joined: 8/23/2024 Last visit: 2/22/2025 Posts: 3 Rating:
|
Thanks for idea.. |
Follow us on