1/16/2018 11:36 PM | |
Joined: 8/27/2014 Last visit: 9/9/2022 Posts: 10 Rating: (0) |
Dear Sirs, I need to connect several automation panels in a redundant fiber optic ring topology. I have found the following application manual, provided by siemens: https://support.industry.siemens.com/cs/ww/en/view/109739600 My plan is to integrate 2 SCALANCE X308-2M with fiber optic modules (2x MM991-2 (BFOC) in each automation cabinet. One SCALANCE X308-2M will be a part of the master ring and one for the standby link. For the rings I will use one MM991-2 (BFOC) - I attached a picture. In the documentation the 2 rings are connected in 2 places. My question is: Can I connect both rings in each automation panel or like in the application manual, in just 2 places ? Also, for the rings I will use fiber optic. Is a good idea that between rings the connection should be done on fiber optic or is not a real advantage. Thank you! |
Last edited by: mihaiTC at: 1/17/2018 12:08:17 AMLast edited by: Jen_Moderator at: 1/17/2018 11:38:42 AMInserted right link. |
|
Follow us on