11/8/2012 12:30 AM | |
Posts: 1 Rating: (0) |
Hi |
11/9/2012 12:46 PM | |
Joined: 2/14/2012 Last visit: 9/26/2024 Posts: 31 Rating: (10) |
Hi Ivad, The configuration steps with the RF340R and RF380R should been equal to the application description. 1. and 2. issue: Maybe some words to the configuration. You have to check and parameterize the size of your MDS (8 or 24 bytes) into the function block. Here you can find a FAQ with more information to the topic http://support.automation.siemens.com/WW/view/de/34602561 3. To receive or write the data into the Operator Station (WinCC) you have different possibilities: - You can use operator (visualization) blocks like OpAnl from the library - You can change the attributes from the RFID_Para FBIn the case you like to change the attributes: · Change the necessary attributes of the FB. For more information look to this entry’s http://support.automation.siemens.com/WW/view/de/17233975 http://support.automation.siemens.com/WW/view/de/2936808 · After the change of the FB an update of your blocks is necessary · Then a compile of the OS · In the next step, you can include in the OS picture an Input/Output field an interconnect this pictures with the new variables (ou)tputs with S7_m_c attributes |
Last edited by: PatrikStar at: 11/9/2012 2:29 PMLink added Last edited by: PatrikStar at: 11/9/2012 2:23 PMletter size changed Last edited by: PatrikStar at: 11/9/2012 12:47 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on