11/15/2019 2:39 PM | |
Joined: 8/31/2005 Last visit: 5/21/2024 Posts: 2197 Rating: (326) |
You read the dataset 0. This dataset includes identification data. So I can understand nothing changes. In dataset 0 in the Bytes 7 and 8 the Verndor ID (11) and in the Bytes 9-11 the Device ID (010101) is stored. According https://io-link.com/share/Downloads/Vendor_ID_Table.xml the vendor ID 17 is Endress+Hauser (www.process-solutions.endress.com). The other used datasets of the IO-device must be described in its documentation. So ask Endress+Hauser for it.
|
Last edited by: miami at: 11/15/2019 14:45:45 |
|
11/15/2019 4:21 PM | |
Posts: 25 Rating: (5) |
I would contact the meter's manufacturer to get the correct Index number. |
11/17/2019 3:57 PM | |
Joined: 10/2/2018 Last visit: 2/15/2023 Posts: 8 Rating: (0) |
Please clarify by what you mean by dataset 0 in the first line? |
11/18/2019 5:24 AM | |
Posts: 1283 Rating: (105) |
Maybe this attachment from PicoMag helps
AttachmentPicomag IO-Link.pdf (283 Downloads) |
This contribution was helpful to1 thankful Users |
11/18/2019 8:15 AM | |
Joined: 10/2/2018 Last visit: 2/15/2023 Posts: 8 Rating: (0) |
It seems the ISDU (hex) values are the indexes. So thanks to everyone. |
Follow us on