1/9/2008 12:00 PM | |
Posts: 6 Rating:
|
Hi, I'm new in this forum.I have a project with 2 redundant Cpu 315-2dp with 2 OLM/G12 and 5extensions with ET 200M. On each extension I have 2 IM 153-2 FO(6ES7 153-2AB02-0XB0 redundant). Actually, I want to have redundant optical rings connection. The CPU will connect to OLM and link up all IM153 FO via FOC ; my question is that IM153-2 FO support redundant rings. Is it work If I connect like this way, pls refer to attach file. AttachmentTOPOLOGY_FORUM.zip (710 Downloads) |
Last edited by: CS Moderator at: 09.01.2008 18:59new subject after splitting |
|
1/10/2008 4:17 AM | |
Posts: 6 Rating:
|
Hi PeteB & Late, Thanks for the comments and advice. I know what to do....Thanks again. |
1/10/2008 12:11 PM | |
Posts: 16 Rating:
|
Jack, The OLM/G12-1300 supports 50/125µm or 62.5/125µm(multimode) FO cable upto 10kmor 10/125µm (single mode) FO cable for upto 15km. I guess it depends on what the max distance is you need to cover. Here is the link to the OLM V4.0 manual that contains this tech data: http://support.automation.siemens.com/GB/view/en/24164176 |
Follow us on