4/30/2016 2:07 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Hello, probably this link can help you: |
With best regards... |
|
4/30/2016 2:09 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Yes it will work. Permitted ambient conditions = -40 deg cent to +75 deg centg Please check this data sheet PB FC STANDARD CABLE GP SOLD BY THE M |
4/30/2016 2:13 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, The Siemens PROFIBUS cable is intended for fixed installation in buildings or in an environment which is protected from the climate (in-house cabling). The combination of twisted wires, foil shield and braid shield make the cable particularly suitable for industrial environments subject to electromagnetic interference. The design of the cable also guarantees stable electrical and mechanical characteristics after the cable has been installed. Permitted ambient conditions: Operating temperature – 40 °C + 60 °C Transport/storage temperature – 40 °C + 60 °C Installation temperature – 40 °C + 60 °C |
Eng.Mohamed Ibrahim |
|
4/30/2016 2:13 PM | |
Joined: 9/18/2013 Last visit: 2/20/2024 Posts: 203 Rating: (12) |
Hello, You can find the Permitted ambient conditions of SIEMENS PB cable in the attached Picture Also the whole datasheet is here |
Last edited by: Ibrahim Fathy at: 4/30/2016 2:18:31 PM |
|
4/30/2016 2:21 PM | |
Posts: 32 Rating: (4) |
Thanks All, This is Really helpful Vaibhs. |
This contribution was helpful to1 thankful Users |
4/30/2016 2:32 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Kindly find the attached file. |
Eng.Mohamed Ibrahim |
|
Follow us on