7/11/2012 8:45 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928) |
Hello, I want to save all manuals (especially pcs7 ) to my disk. In the folder C:\Program files\SIEMENS\Documentation\English are all manuals, except they are all shorcuts. The original file name is something like: s7jil71b.Is there a link or something to download all at once with logical names? The manuals on the DVD have logical names, but are not complete My documentation manager is not helping either... |
If I could help you, you can use the RATE button. Thank you. |
|
7/11/2012 4:11 PM | |
Posts: 836 Rating: (100)
|
Check the manual collection: https://www.automation.siemens.com/mcms/industrial-automation-systems-simatic/en/manual-overview/tech-doc-pcs7/Pages/Default.aspx?HTTPS=REDIR The file names are not like "PSC 7 Engineering Whatever", you have to rename it by yourself, or just use folders named that way. |
This contribution was helpful to1 thankful Users |
7/12/2012 9:21 AM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
Or you can run my VBScript, which copies all pdf documents from that list of shortcuts to C:\SIEMENS and applies new names according to the names of those shortcuts. Tested on PCS 7 v7.1 SP3 AttachmentCopyRename PCS Documentation v1.0.zip (48 Downloads) |
Last edited by: TerminalBuzz at: 7/12/2012 9:22 AM |
|
This contribution was helpful to2 thankful Users |
7/16/2012 9:54 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928) |
SilentBob, that is excactly what I dont want to do...open pdf, take name from title, close, rename, copy to directory and that x55.. no thanks TerminalBuzz, thanks man this is exactly what I needed!! Did you get the filename locations from some document or did you enter them manually? |
If I could help you, you can use the RATE button. Thank you. |
|
7/18/2012 11:54 AM | |
Posts: 836 Rating: (100)
|
Good job! |
Follow us on