5/19/2013 11:25 PM | |
Joined: 5/27/2012 Last visit: 6/8/2022 Posts: 3 Rating: (0) |
I was thinking that my problem with the e-mail was the port because my server of mail have a different port from 25, but it is not the problem. I have created my own server of mail, have tried with outlook and it works perfectly, when sending the e-mail from the Siemens 1212 appears the following mistake: Requested SMTP connection from 192.168.1.251 16/05/2013 21:25:00 - Error: [10054] Connection reset by peer 16/05/2013 21:25:00 - SMTP connection with 192.168.1.251 ended. ID=13 it is necessary to configure anything more that: ADDR_MAIL_SERVER, WATCH_DOG_TIME, USERNAME, PASSWORD, FROM and TO_S I attach my project, the username is alberto, the password 1234, the IP of the web server 192.168.1.8, PLC IP 192.168.1.251 and the email alberto@localhost.com If anybody find the fault, please contact me. Attachmentema.zip (321 Downloads) |
5/27/2013 12:14 PM | |
Posts: 3 Rating: (0) |
Hi Can i send the Email with the TCP connect or i need GPRS? |
Follow us on