8/13/2023 7:53 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, It looks like you have SELFRESET set to 1. After Completed, the SFC will reset itself to Idle. Completed signal is given, but it's only a pulse for the duration of the OB the SFC runs in. If you set SELFRESET to 0, the SFC remains in Completed state until you set Reset to 1 (in automatic mode). |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
8/14/2023 4:55 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, A new START trigger will also work yes |
If I could help you, you can use the RATE button. Thank you. |
|
8/14/2023 6:34 AM | |
Joined: 1/27/2022 Last visit: 10/13/2023 Posts: 8 Rating: (0) |
The solution worked. Thanks! |
This contribution was helpful to1 thankful Users |
Follow us on