4/1/2016 4:26 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928) |
Hi Berg, In WinCC explorer are pdl's starting with: "@pg_@sfc". These are the faceplates of the SFC. SFC's are shown by a ActiveX component, so it's a bit different from normal block icons, but you can edit them the way you like (to a certain height). For your next question: You can open a pdl, insert an button and while you select the button, you can go to the Dynamic Wizard toolbar, select SFC and then select: "Configure SFC button". When you follow directions, a script is generated and it will show the selected SFC. You can use that script in the screen object. |
Last edited by: Oreca at: 4/1/2016 4:28:00 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on