12/24/2008 1:46 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1426) |
Hi, if I understand, you have a angle in radians (x), and you do a sine function of it [ sin(x) = y]. Now you have the result (y) and would like to find the original angle (x). I'm right? If yes, use arcsin function: if y=sin(x) then x = arcsin(y) in the same way if a=arcsin(b) then b=sin(a) note: in STEP 7 the function arcsin is ASIN. There is no direct command to MicroWin. However take a look at the freeware library at http://support.automation.siemens.com/BR/view/en/19308841 |
Last edited by: Pegaia at: 12/24/2008 1:52 PMDenilson Pegaia |
|
This contribution was helpful to1 thankful Users |
12/28/2008 9:38 AM | |
Posts: 3 Rating: (0) |
Hi Pegaia Yes, that is exactly what i needed. The downloaded link works 100%. Thanks KLR |
Follow us on