11/8/2019 11:14 AM | |
Joined: 2/8/2018 Last visit: 3/28/2023 Posts: 256 Rating: (4) |
No Answer from anyone>????????? |
11/8/2019 5:13 PM | |
Joined: 3/9/2018 Last visit: 5/20/2024 Posts: 182 Rating: (14) |
S7 200 has a highspeed counter (HSC) of 20khz (224XP 200Khz) See S7-200 Programmable Controller System Manual (6ES7298-8FA24--8BH0) You need to calculate the max rpm based on the encoder resolution and max input frequency. |
11/14/2019 6:09 AM | |
Joined: 2/8/2018 Last visit: 3/28/2023 Posts: 256 Rating: (4) |
Thanks for the reply, Firstly i want to specify its , S7 200 smart and not S7 200 . Secondly, do you mean that the encoder series I have mentioned( E50S 8-2000- 3) will not work with smart PLC(ST60)?????????? and i should take as suggested by you {E50S 8-2000-2 (or 3)-V (or T)-24-C} ?????? Please reply. |
11/14/2019 6:09 PM | |
Joined: 3/9/2018 Last visit: 5/20/2024 Posts: 182 Rating: (14) |
Hi, See the datasheet of the E50S on the different part numbers I mentioned |
Last edited by: Henry1675 at: 11/14/2019 18:09:39Last edited by: Henry1675 at: 11/14/2019 18:12:13 |
|
Follow us on