9/29/2008 9:39 AM | |
Posts: 17 Rating: (0) |
Hi everyone, Can anybody help us give any idea for the CP 243-1IT to connect or communicate to the SNMP protocol system. Thanks in advance, Bisaya |
9/29/2008 10:22 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
hello best regards |
Last edited by: UMENCHO at: 9/29/2008 10:24 AM |
|
10/2/2008 3:31 AM | |
Posts: 17 Rating: (0) |
Hi, I need to interface the CP-243-IT to the ASG Sentry program http://www.asg.com/products/product_details.asp?id=96&Code=SNM A web based network monitoring that communicate remote devices that supports SNMP/MIB. Regards, Bisaya |
10/2/2008 4:46 PM | |
Posts: 49 Rating: (5) |
Hi, I had a quick look at the ASG-Sentry specs, it will support TCP and ICMP, perhaps it can be configured to gather some information from the CP using those, even if it's just a ping! I have a 243-1IT online and you are welcome to use it for testing. |
Last edited by: marcsinclair at: 10/2/2008 4:48 PMforgot the http:// :) |
|
Follow us on