5/2/2012 11:44 AM | |
Joined: 2/5/2009 Last visit: 3/19/2024 Posts: 36 Rating: (1) |
Hello, I'm trying implement a solution but I have some doubts on what is the best architecture. The solution consists of two separate systems, each has its controller and one controllers have a remote unit acquisition. In the HMI of each cabine is intended to show information on the two controllers. In the architecture option1 it's easy to do, i configure 2 connnections in HMI for each controller. In the architecture option2 it's more hard, because share information between the controllers using ethernet connection. What do I need to know is if the architecture of option 1 is correct or not. The architecures are in attach files. Someone can help me? Regards AttachmentArchitectures.zip (76 Downloads) |
5/2/2012 12:32 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Answer of your questions is yes. Useful FAQs =Which PROFINET nodes support the extended PN diagnostics and what do you have to configure? Best regards, Hristo Mihalev
|
This contribution was helpful to2 thankful Users |
Follow us on