1/11/2012 11:16 AM | |
Posts: 26 Rating: (0) |
No solution from me, but I am struggling with the same problem. Fail to understand why an new software, i.e. TIA would make stuff work worse?
|
4/4/2012 10:47 AM | |
Posts: 24 Rating: (0) |
Any progress on this one? Is there a software update solving this problem? Maybe I SP3 available? I’m attending to upgrade from wincc 2008 to wincc v11. I really need this transparency function because I’m making a costume made simulation. The reason for my upgrade is, I need to program a SIMATIC HMI TP900 Comfort. In wincc 2008 I knew that not every device type supports transparency on the Graphics view. For example: -> The Basic panels doesn’t. -> The OP 270 10" does. I don't know if the TP900 comfort supports this anyway? |
4/6/2012 9:25 AM | |
Posts: 24 Rating: (0) |
I guess he means: When you import an .WMF image with a transparent background in to an graphic view. |
Follow us on