11/30/2016 4:41 AM | |
Joined: 2/20/2014 Last visit: 5/9/2024 Posts: 395 Rating: (38) |
Hi there, I was trying to update the firmware for CMR2020 (I had choosed the path where the firmware update file is located in my laptop the i had clicked on the "LOAD" button. And i had encountered something which i think is unusual (The uploading status was 65% then after some time, i was automatically logged out of the WBM). Attached is the screenshot of what i can see after i login again into the CMR. Please advise what needs to be done next as i can see that the status showing "Format error". Thank you in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/30/2016 4:07:15 PMNew subject after splitting |
|
11/30/2016 5:03 AM | |
Joined: 12/18/2014 Last visit: 5/24/2024 Posts: 33102 Rating: (4085)
|
In your place I would start a support request. |
This contribution was helpful to1 thankful Users |
11/30/2016 5:04 AM | |
Joined: 2/20/2014 Last visit: 5/9/2024 Posts: 395 Rating: (38) |
I managed to update the firmware successfully after several try. |
11/30/2016 7:50 AM | |
Joined: 12/18/2014 Last visit: 5/24/2024 Posts: 33102 Rating: (4085)
|
|
This contribution was helpful to1 thankful Users |
11/30/2016 9:06 AM | |
Joined: 2/20/2014 Last visit: 5/9/2024 Posts: 395 Rating: (38) |
I have now created a support request. Thank you for your advise. |
This contribution was helpful to1 thankful Users |
2/7/2018 1:46 PM | |
Joined: 6/19/2017 Last visit: 5/24/2024 Posts: 8084 Rating: (165) |
New question published by VictoriaLorenzo is split to a separate thread with the subject What can do to receive the emails?? . Best regards |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on