1/21/2025 10:15 AM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi Aivars, In this case, you will have to install the software again. In the LSC there is no software license as such, it is included in the installation DVD that you get when you order it. Therefore, you have to install the DVD 100%. Best regards!
|
If this Information really helps, you could use the Rate function |
|
1/21/2025 2:12 PM | |
Joined: 9/11/2014 Last visit: 9/16/2025 Posts: 868 Rating:
|
Hi, if you have a original LOGO! Soft Comfort DVD, then officially you have the license and the right to use it. The Demo version is seperate. You now can install from DVD, or you install the LOGO! Soft Comfort V8.4 SP1. Link to upgrade LOGO! Soft Comfort V8.4 SP1 If you have installed a LOGO! Soft Comfort version on your PC, then you do not need to insert the original LOGO! Soft Comfort DVD. Hope this helps |
Follow us on