11/7/2012 5:34 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (714)
|
Hello, You can use the buildin High speed counters of the PLC, use the wizard for the setup. Attached an example how to use the counters for positioning. regards, Marcjan AttachmentHSC_ex.zip (786 Downloads) |
Problem solved? |
|
12/31/2013 3:35 PM | |
Joined: 9/1/2005 Last visit: 8/1/2024 Posts: 4104 Rating: (194) |
follow up question published by alfeturiis split to a seperate thread with the subject help for wiring of two plus four wires DC motor shaft encoder Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
1/2/2014 4:27 PM | |
Posts: 204 Rating: (1) |
you can use HSC (High speed counter ) wizard in microwin and see help of microwin to select which mode u need . and which type u want |
3/6/2015 9:35 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4769 Rating: (123) |
|
Follow us on