9/13/2014 4:24 PM | |
Posts: 784 Rating:
|
Thanks William. But what happen for Logo V8 if we remove Logo V7 in this case"no need for it"? |
9/13/2014 6:28 PM | |
Posts: 5225 Rating:
|
Honestly, I would probably just let it stay there. But let's say one of the PCs needs to be cleared for some reason, the steps would be.. * Create a Windows restore point, for just in case. * Backup the latest registry entries. * Use WiseProgramUninstaller to safely and cleanly uninstall V7. * Reboot the PC. * Test if V8 is still working. If working (which I believe it will) then good, else... * If not working then try to restore V7 with the Windows restore point. Else.. * If that does not work - uninstall any traces of V7 and V8 * Install V3 from my original install disk * Upgrade to V8 * Check upgraded V8 version to be working * Check if V3 still operational.. leave in place if not removed. Honestly.. I do not know what to suggest to you for 100% risk free. You would be most welcome to roll the dice with Support Request. Regards. w |
This contribution was helpful to
1 thankful Users |
9/13/2014 7:53 PM | |
Posts: 784 Rating:
|
Hello William, Iam afraid to do this. If any member can do,inform us with the results. Best regards....... |
Last edited by: Wago at: 9/13/2014 8:05 PM |
|
9/13/2014 8:35 PM | |
Posts: 784 Rating:
|
Hello 190B, V8 can open the application programmed by previous versions,otherwise impossible. true or false? Best regards.... |
Follow us on