4/5/2016 7:22 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hi, Are you getting feedback from your simulation driver? You can try setting: NoFbkOpen and/or NoFbkClose to check if the feedback is the giving the error.... And if that is not working either, you can upload a screen of the cfc chart (in test mode), so we can take a look on the configuration... |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/5/2016 8:02 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hi, In the rectangle you are referring to is reserved for status signals like simulation, maintenance, time monitoring error etc. A extended status display is used for this. You better can use ExtMsg1-3 to call additional messages |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on