12/22/2021 12:07 PM | |
Joined: 12/21/2021 Last visit: 2/23/2022 Posts: 2 Rating: (0) |
Hello there.. I tried to apply the method ..and it worked..no more start /stop signals are getting generated.. now the problem is..when I turn feature bit high and localsetting =2 ,it Grey's out local mode selection in faceplate..now I can't switch to local mode using the faceplate..but if I keep localsetting=4 and feature bit 20 high ..faceplate allows me to select between local,manual,automatic mode. But when feature bit is high and localsetting=4 is kept and at that time if fbkrun becomes 0 then there's no P_stop signal generating.. Can u just help me out with this configuration..I want P_stop when fbkrun becomes 0,but no P_start when fbkrun becomes 1.. Just tell me it's possible 👉👈
------------------------------------------------------------------------------------------ |
Last edited by: mananthakor2 at: 12/22/2021 12:29:45Last edited by: Jen_Moderator at: 12/22/2021 13:45:00New subject after splitting |
|
Follow us on