5/16/2011 1:51 PM | |
Posts: 59 Rating: (0) |
i need your help i'm stuck up on site.... I'm using 2 414-3H CPU and 6 IM CPu with WinCC 7.0 SP1. 1. CPU1- 414-3H CPU 1 is Exchanging data with CPU-2. (400 bytes) The whole n/w of 2 H-cpu's and 6 IM's and 2 work stations are connected on the same n/w using the fiber optic. My Issue is when i activate 1st work station the 2nd gets disconnected i.e. the connection is lost. with the same settings, changing nothing, i deactivate the 1st which i activated and having healthy connection, the 2nd work station becomes healthy. Now i activate the 1st again, now it gets activate but its connection status is disconnect. Now again i disconnect the 2nd one, the 1st becomes healthy. i can get only 1 work station healthy at a time with the same settings on both stations, and changing nothing settings, with same settings it gets healthy status switch. that which station i activate 1st it will become healthy, other 1 will show disconnected. waht is the problem i'm not getting. pl if anybody knows the solution, pl help me this problem is very critical for me... waiting for ur positive reply. Regards, AttachmentNetwork.zip (70 Downloads) |
Last edited by: Ammu at: 5/16/2011 2:33 PMLast edited by: O_Moderator at: 5/16/2011 2:11 PM |
|
5/16/2011 2:12 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already discussed in the following thread winCC connection problem. Best regards O_Moderator |
Follow us on