1/16/2020 12:45 PM | |
Joined: 3/14/2008 Last visit: 5/29/2024 Posts: 2070 Rating: (928)
|
Hi, it looks like your screen resolution is different from the WinCC screen settings.. Please check your screen resolution and adjust it in the OS project editor in WinCC Explorer. It will scale the WinCC HMI screen to your screen resolution. To answer your question: Go to WinCC Explorer and under Computer select the computer name and right click->Properties. Go to tab: Graphics Runtime and under Window attributes you can select the desired functionality. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
7/17/2020 9:48 AM | |
Joined: 8/1/2019 Last visit: 5/29/2024 Posts: 299 Rating: (3) |
Thank you, for the answer but it didnt help so far. |
Follow us on