2/8/2010 12:56 PM | |
Posts: 96 Rating: (7) |
Hi, Can I use commercial ethernet cards instead of CP1613 ? BR |
Last edited by: Raednabeel at: 2/9/2010 8:06 AM |
|
2/9/2010 3:35 PM | |
Posts: 96 Rating: (7) |
Dear Darius, The second method is used in software redundancy, and I had used it . See the attached for a PDF. When I had implemented the method , I did not find any thing relates it to what is existed in the PLCs side. All what it dose is to generate a global C action, this will change the connection parameters to pre-configured ones in order to connect with the other PLC. So , my question is why it will not work instead of the first method ? especially it is easier and cheaper ! AttachmentSWR_WINCC_english.zip (679 Downloads) |
Last edited by: Raednabeel at: 2/9/2010 4:00 PMLast edited by: Raednabeel at: 2/9/2010 3:38 PM |
|
This contribution was helpful to1 thankful Users |
2/10/2010 10:48 AM | |
Posts: 378 Rating: (47) |
Just for the people who can´t open Raednabeel´s .zip-file: You have to rename it as .rar-file than you can open it. best regards bilao |
This contribution was helpful to1 thankful Users |
Follow us on