3/7/2024 7:44 AM | |
Joined: 7/15/2023 Last visit: 4/15/2024 Posts: 9 Rating: (0) |
I have TIA v17, winCC RT Pro SCADA system for CPU S7-1200 (1214DC/DC/DC). I am facing following issues, request to kindly help. 1)The SCADA system only log trends for one day only (after runtime starts). After that (next day) the trends not log and when we open the trend page, only current trend shows and previous history is not showing. 2) WinCC RT unable to stop normally. Whenever we want to stop runtime, error message shoes- "No more threads can be created in the system" or sometimes ""RPC server is unavailable". Please help me out to resolve the issues. I have attached photo for reference only. AttachmentTIA17 WinCC RT Pro logging issue.pdf (79 Downloads) |
3/18/2024 6:24 AM | |
Joined: 7/15/2023 Last visit: 4/15/2024 Posts: 9 Rating: (0) |
Hello Murof, 1) TIA v17 update 6 & WinCC RT Pro v17 update 6 2) OS- Windows 11 Pro 64bit 3) I have created the runtime file from TIA v17 & then this file is run from WinCC RT Start. 4) In archive manager folder, database are created for only one day, i.e., day when project is started. Please refer to photos in attachment and suggest possible solutions to resolve the issue.
AttachmentTIA17 archive detail.pdf (2 Downloads) |
Last edited by: SEETI-I at: 03/19/2024 06:01:40 |
|
Follow us on