4/7/2025 10:45 AM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello! The first thing I would check would be that the Windows 11 version is not the latest 24H2, which is not tested for compatibility with WinCC 7.5. The exact version you can see with "Windows + R" and typing winver. Also, only WinCC 7.5 with SP2 is the one that can have compatibility with some versions of Windows. 11. I attach the excel that I have obtained from the Compability Tool in case you want to check it. I hope this comments help 🍀 AttachmentWinCC_V7.5_compatibility-list_en_2025-03-13.xlsx (185 Downloads) |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on