8/23/2012 11:00 AM | |
Joined: 2/10/2010 Last visit: 8/6/2024 Posts: 22 Rating: (0) |
Hi.I developed some WinCC V7 application for sewage pump station network (all stations are same). Didn’t work before with faceplates and didn’t have time to test and learn so I’ developed application without faceplates. I can say that it was a nightmare to change hundreds of tags. Now I’m trying to learn how to make smarter solution using faceplates. Whit some other manufacturers (e.g. Allen Bradley) you can create one graphic file and then call each time same graphic file but with other tags (defined with some text file). I’ was hoping that faceplate is the same thing. I created some faceplate where I have some graphics objects which should change depending on some tags (VB scripts). But now, when I want to use it in WinCC pdl, I don’t know how to link internal faceplate tags with external WinCC tags . Is this possible? So my idea is to cerate one faceplate I call it in WinCC with different tags (for each station). Please find attached my faceplate file.I’ looked at some post on this forum ¸and try Komi’s sample but still I don’t have answer for my question. Thanks Regards Alen AttachmentC:\Users\Public\Documents\Siemens\WinCCProjects\Brdovec\Brdovec2\GraCS\CS.zip (483 Downloads) |
8/23/2012 12:43 PM | |
Posts: 1776 Rating: (95)
|
Hi, you can use the 2 wizards Creating faceplate as a type creating instances in the plant picture see WinCC online help chapter Working with WinCC > process Picture Dynamics > Dynamic Wizard > Picture Components See also the application http://support.automation.siemens.com/WW/view/en/31624179 |
Follow us on