1/19/2018 12:02 PM | |
Joined: 10/14/2010 Last visit: 8/7/2024 Posts: 59 Rating: (3) |
Hi, I've been given a project that someone else has designed and left me to configure. Unfortunately they are not contactable for a few days so I was wondering whether anyone would be able to tell me if this topology (see attachment) is even possible? Is it possible to use 4 X204-2's (FW5.2) in a redundant ring using the fibre ports, with 3 of the switches also hosting their own ring using ports 1 & 2? ((Please attached pdf of the topology I'm trying to explain) I'm using TIA V14 SP1, in the properties of the switch it look like I can only configure one MRP ring? It can be either the client of the fibre ring or the master of it's own ring, not both? Is that correct or am I missing something? Thanks in advance Rich Attachmentscanned-20180119115737.pdf (120 Downloads) |
4/23/2018 11:12 AM | |
Posts: 2 Rating: (0) |
Hi, how did you solve the situation? |
11/13/2018 8:15 PM | |
Posts: 4 Rating: (0) |
|
Last edited by: Ramky89 at: 11/14/2018 5:02:20 AM |
|
11/13/2018 8:20 PM | |
Joined: 12/18/2014 Last visit: 8/14/2024 Posts: 33557 Rating: (4168) |
Hello Ramky89, please be so kind and don't post twice for the same problem. https://support.industry.siemens.com/tf/de/en/posts/x204-2/202720/?page=0&pageSize=10 |
Last edited by: ixo65 at: 11/13/2018 8:22:33 PM |
|
Follow us on