1/26/2009 9:46 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hello Is this for your case valid? What should you watch out for if you want to use a function module FM458-1 DP (6DD1607-0AA2) with expansion module EXM448? reagrds |
1/26/2009 6:31 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating:
|
Hello xingyunxing, the FM458 can be used with a EXM448 or a EXM448-1. The difference between the EXM448 and a EXM448-1 is the Simolink module slot. On the EXM448 is emty, on the EXM448-1 a Simolink module is pluged in. It it possible to add a Simolink module to the EXM448, this makes itequal to a EXM448-1. In HW Konfigyou have to define the slot is in use or not, see properties.jpg PS: happy new year AttachmentEXM448(-1).zip (429 Downloads) |
|
|
2/5/2009 6:01 PM | |
Posts: 7 Rating:
|
my EXM448-1 have only a green led flash after downloading *.2bfconfiguring file. The SLB on the EXM448-1 have only a red led flash.As long asi connect EXM448-1 with FM458,FM458 can not not start up normally,after downloading pragram,arise dialog box "stop(initialization error)" . AttachmentEXM448 TEST.zip (441 Downloads) |
Follow us on