9/18/2024 9:06 AM | |
Joined: 5/30/2014 Last visit: 9/18/2024 Posts: 147 Rating: (18) |
Hi, I have installed a Library of general functions (LGF) for SIMATIC STEP 7 (TIA Portal) and SIMATIC S7-1200 / S7-1500 for TIA v.16. I must say that this is my first such lib installation. I extracted a downloaded zip to the new folder and installed navigating to the LGF.al16 file from here: It seems that it is installed well because I could compile the whole program without errors and get the tooltips when hover over the FB pins. However, if I select the block and press Ctrl-F1, the help is opened in a (default) browser. 1. I expect that help for LGF functions is opened in the global help window ("Information system") of TIA instead in the browser. Is it possible at all? Thank you in advance. |
Last edited by: C-3PO at: 09/18/2024 09:08:06Last edited by: Moderator_Lan at: 09/18/2024 10:37:28link optimized If you find my contribution helpful please RATE it :)) |
|
Follow us on