10/20/2018 5:00 PM | |||||||||||
Joined: 3/28/2015 Last visit: 5/25/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topics might help:
2- CPU Default IP Address : 0.0.0.0 Turning off Fire wall and Anti-virus Connect PC directly to CPU Start accessible Nodes in TIA Software Assign IP Address Or Use "Proneta" to assign IP Address 3-SIMATIC S7 S7-1200 Programmable controller Assigning or checking the IP address of your programming device using "My Network Places" (on your desktop)To assign or check your programming device's IP address, follow these steps:
You can now connect to the CPU.
|
||||||||||
Last edited by: Jen_Moderator at: 10/22/2018 10:28:34 AMOptimized links. Eng.Mohamed Ibrahim |
|||||||||||
10/20/2018 5:22 PM | |
Joined: 3/28/2015 Last visit: 5/25/2024 Posts: 721 Rating: (213) |
Hello, Configure the HW in your program with CPU V4.1 and download it to CPU V4.2 and accept the warning message. |
Eng.Mohamed Ibrahim |
|
10/20/2018 5:50 PM | |
Joined: 3/28/2015 Last visit: 5/25/2024 Posts: 721 Rating: (213) |
Hello, 1-The warning message when you Configure the HW in the program with CPU V4.1 and download it to CPU V4.2 2-Use "Proneta" to assign CPU IP Address |
Last edited by: Jen_Moderator at: 10/22/2018 10:29:31 AMOptimized link. Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
10/20/2018 7:47 PM | |
Joined: 3/28/2015 Last visit: 5/25/2024 Posts: 721 Rating: (213) |
Hello, TIA V13 Software is incompatible with the firmware V4.2 There is no problem to configure the HW in the program with CPU V4.1"Programmed"and after the communication with CPU,you can download the program to CPU V4.2"Actual" The software will give you a warning message that there is a mismatch between actual and programmed hardware. You can ignore this message and continue the download. |
Eng.Mohamed Ibrahim |
|
Follow us on