3/26/2012 1:44 PM | |
Joined: 4/6/2006 Last visit: 6/24/2025 Posts: 604 Rating:
|
Hi Rosegarden, I'm not 100% sure but could it have something to do with the display mode of the LEDs you have set? See Chapter 7.4 and 7.5 of the following manual: SIMATIC NET Industrial Ethernet Switches SCALANCE X-300 Operating Instructions This mode can be changed by pushing the SET/SELECT Button briefly. Meaning of the LED in Display mode: L1/L2: Status off Power supply L1 / L2 is not monitored. If L1 / L2 falls below 17 V *), the signaling contact does not respond. |
Best regards, |
|
Follow us on