6/6/2011 12:07 PM | |
Posts: 103 Rating: (0) |
HI EVERYONE what is the benefit to unlink the db and how it is possible thanks |
6/6/2011 12:12 PM | |
Posts: 691 Rating: (37) |
May be this thread will help you https://www.automation.siemens.com/tf/WW/en/Posts/45535 |
6/7/2011 8:22 AM | |
Joined: 10/7/2005 Last visit: 10/18/2024 Posts: 3024 Rating: (1054)
|
Both can be used (SFC20 OR SFC83)and apart from the link thatdchartier listedin the threadthat Sharrefered too, the following may prove useful too: How can the program runtime be optimized if the main memory of the CPU is too small for the runtime-relevant STEP 7 program?" |
Last edited by: fritz at: 6/7/2011 8:25 AMCheers |
|
6/7/2011 8:29 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Both can be used (SFC20 OR SFC83)and apart from the link thatdchartier listedin the threadthat Sharrefered too, the following may prove useful too: How can the program runtime be optimized if the main memory of the CPU is too small for the runtime-relevant STEP 7 program?" Dera fritz Thanks for confirming that SFC20 can be used. i got confused for a while. Now it is clear that both SFC can be used. |
VANDE MATARAM..... |
|
Follow us on