8/14/2017 8:22 AM | |
Posts: 12 Rating:
|
Hi, fluidcontrol. Thanks for your reply. I have solved this problem almost as you recommended but some another way: In HMI Alarms took empty field, for example, "Additional text 1", and dublicate to this field value which in field "Alarm group". And in Alarm view -> Properties ->Alarm filter set filter to field "Additional text 1" in lieu of "Alarm group". It is a crutch but it works. There are once more issue that I can't resolve: I need to count number of alarms in different classes and groups. But I need to do it in script (C or VB doesn't matter) and start this script with some event or timer. I have considered functions which having in WinCC scripting but nothing till found. Can you some advice for this matter? New question published by sna8810_0s is split to a separate thread with the subject Count number of alarms in different classes and groups - Which functions can use for this?. Best regards |
Last edited by: sna8810_0s at: 8/14/2017 2:11:24 PMLast edited by: Jen_Moderator at: 8/14/2017 2:19:18 PMCrossed out second question. Second question is published in a new Thread. Last edited by: The Helping Hand at: 9/8/2017 1:06:25 PM |
|
Follow us on