5/3/2019 9:39 AM | |
Joined: 8/3/2016 Last visit: 1/19/2022 Posts: 21 Rating:
|
Yes ID1000 is DINT which then i multiply by -1 for other direction, then DINT to REAL conversion and finally multiplication with 0.05 for correct linear measure, or at least i would like to because PLC malfunctions as soon as i insert any of those blocks This is demonstration of what happens when any of those blocks are downladed to CPU: [snip] You can see that M0.0 marker is set by EMG pushbutton but only M0.0 in Networks 1 and 2 are set In other networks are not but its the same marker Sometimes few outputs oscillate, turn on and off randomly, different markers are set or reset without any permission I installed update 4 yesterday and same thing is present AttachmentCpu-20190503T094006Z-001.zip (529 Downloads) |
Last edited by: Jen_Moderator at: 05/03/2019 11:41:56Removed link and added file as an attachment. |
|
Follow us on